Recommendations for Linux-Based Devices for Building LoRa/LoRaWAN Gateway with RAK5146

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommendations for Linux-Based Devices for Building LoRa/LoRaWAN Gateway with RAK5146

1,435件の閲覧回数
BinaryNomad
Contributor I

Hola NXP Community,

We are currently using the RAK Wireless RAK5146 module to build a LoRa/LoRaWAN gateway. While we are familiar with Raspberry Pi as a commonly used platform for this purpose, we are exploring other suitable Linux-based devices that are compatible and reliable for gateway development.

Could you kindly share your recommendations for alternative Linux-based systems (e.g., SOMs, SBCs, or industrial PCs) that would work well with the RAK5146 for both LoRa and LoRaWAN functionalities? Additionally, any specific part numbers or models you have successfully worked with would be greatly appreciated.

タグ(3)
0 件の賞賛
返信
1 返信

1,356件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @BinaryNomad 

I hope you are doing very well.

 

I believe any Linux based device can handle this kind of LoRa devices, but just you can find/develop the driver for this.

For example, the i.MX93 or in general the i.MX Family are Linux based systems. 

Also, I found this repository with a driver that seems to be for this specific device and it is for Linux.

You can try to cross-compile and test it.

 

Best regards,

Salas.

0 件の賞賛
返信