Re: How can i configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Re: How can i configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11

跳至解决方案
1,107 次查看
Abrar_23
Contributor III

Hello @PavelL, @alejandro_e 

I am Trying to Implement VLAN for Sending Two different Streams such as stream1, stream 2

so for that on top of Existing Configuration I am trying to include VLAN for that

General Parameters Table 

TPID = 34984

TPID2 = 33024

L2 Lookup Table 

I changed the MASK to 

0x1FFFFFFFFFFFFFFFF for including VLAN, IOTAG

MACADDR = 0x4C4C36454143

SRCPORT = 3

DSTPORT = 1,2,5

CB Sequence Generation and Individual Recovery Table

REPLACE_PORT = 1,2

TAG_PORT = 1,2

CB Tag Replacement Table 

REPLACEVLANID - ENABLE

VLANID = 1

RTAG_RESERVED = ENABLE

Second VLAN Integration

 L2 Lookup Table 

I changed the MASK to 

0x1FFFFFFFFFFFFFFFF for including VLAN, IOTAG

MACADDR = 0x112233445566

SRCPORT = 4

DSTPORT = 1,2,3

CB Sequence Generation and Individual Recovery Table

REPLACE_PORT = 1,2

TAG_PORT = 1,2

CB Tag Replacement Table 

REPLACEVLANID - ENABLE

VLANID = 2

RTAG_RESERVED = ENABLE

Added VLAN Lookup Table for both stream 

VMEMB_PORT = 1,2,3,5

BC_DOMAIN = 1,2,3,5

TYPE_ENTRY[0]  = ENABLE

TYPE_ENTRY[1] = ENABLE

This was the change I was planning to have a Separate VLAN ID for this Two Different MAC Address Computation for that I am trying to Implement VLAN?

whether this configuration Satisfy the configuration of VLAN or what are the other changes need to be made for Configuring VLAN ?

0 项奖励
回复
1 解答
1,075 次查看
PavelL
NXP Employee
NXP Employee

Hello @Abrar_23 ,

I moved the post to the thread. I hope I will come with answer this week.

Thank you for your understanding.

Best regards,

Pavel

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,049 次查看
PavelL
NXP Employee
NXP Employee

Hello @Abrar_23 ,

I went through your setup. I apologize but I'm not sure what do you want. Could you please be more specific?

Do you want to tag ingress? Keep tag on egress? Do you want to isolate the CB traffic from the other traffic by adding a VLAN tag to it?

Thank you.

Best regards,

Pavel

0 项奖励
回复
1,032 次查看
Abrar_23
Contributor III

Hello @PavelL 
So, for my setup I am having two Stream say stream 1 & stream 2
when i enable both the stream same time i am losing the stream 1 Packets 
so, in order to overcome this issue i am planning to add VLAN to overcome this issue by the reference from document i read when VLAN is added we will have a Separate queue for Processing each stream since separate VLANID is assigned 
I want to add tag on the Egress 
Yes, I want to Isolate the CB Stream Traffic from other traffic by adding VLAN tag to it 
 I tried the above implementation i checked the ethernet Frame where the VLAN ID is tagged but its unable to overcome the issue of Packet loss of Stream 1 when both the stream is append running 
assigned different VLANID and VLAN(Priority) different but the still packet loss is happening 
How to overcome this issue 
Regards
Abrar 

标记 (1)
0 项奖励
回复
1,009 次查看
PavelL
NXP Employee
NXP Employee

Hello @Abrar_23 ,

let's start with the CB.  If you want to isolate the CB traffic from the other traffic by adding a VLAN tag to it, you have to do the following:

 

Add VLAN entry to VLAN Lookup Table

 // no mirroring

VING_MIRR = 0x0

VEGR_MIRR = 0x0

// vlan port membership, add ports used for CB

// for switch 1 this would be e.g. port 2, 3 and 4

VMEMB_PORT = 0x1C

VLAN_BC = 0x1C

// keep the VLAN tag at egress

TAG_PORT = 0x1C

// VLAN type this entry is eligible for

TYPE_ENTRY[1] = 1

TYPE_ENTRY[0] = 1

// VLAN ID

VLANID = 100

 

Edit the respective L2 Lookup Table entry

// add VLAN ID 100 to the lookup

VLANID = 100

VLANIDMASK = 0xfff

where VLANIDMASK is a part of MASK, you already have set up.

 

If you want to keep VLAN tag on egress, select port in TAG_PORT (VLAN lookup table).

If you want to add VLAN tag on ingress, VLANID shall be set on MAC configuration table for the requested port.

I think that L2 policing table shall be also set - please check AN12925, chapter 5.3.1 L2 policing.

Your idea with VLAID priority as the flow shaper might work.

BTW, how do you generate your streams? How much traffic (Mbps) do you generate?

Bets regards,

Pavel

0 项奖励
回复
990 次查看
Abrar_23
Contributor III

Hello @PavelL 
SWITCH - 1

Initially Created a Default VLANID 
VLANID = 0
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Disable all Ports
BC_DOMAIN = Disable all Ports
TAG_PORT = Disable all Ports
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 0

VLANID = 1
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4 -- ENABLE
BC_DOMAIN = Port 1,2,3,4 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 1

VLANID = 2
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4,5 -- ENABLE
BC_DOMAIN = Port 1,2,3,4,5 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 2

MAC Configuration Table 
Port 1 --> VLANPRIO = 7
VLANID = 1
Port 2 --> VLANPRIO = 7
VLANID = 2
Port 3 --> VLANPRIO = 7
VLANID = 3
Port 4 --> VLANPRIO = 7
VLANID = 4
Port 7 --> VLANPRIO = 3
VLANID = 2

SWITCH - 2
VLANID = 0
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Disable all Ports
BC_DOMAIN = Disable all Ports
TAG_PORT = Disable all Ports
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 0

VLANID = 1
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4 -- ENABLE
BC_DOMAIN = Port 1,2,3,4 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 1

VLANID = 2
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4,7 -- ENABLE
BC_DOMAIN = Port 1,2,3,4,7 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 2

MAC Configuration Table 
Port 1 --> VLANPRIO = 7
VLANID = 1
Port 2 --> VLANPRIO = 7
VLANID = 2
Port 3 --> VLANPRIO = 7
VLANID = 3
Port 4 --> VLANPRIO = 7
VLANID = 4
Port 5 --> VLANPRIO = 3
VLANID = 2

can you give me a right way for the above one what are the VLANID need to be configured in MAC Configuration table and VLAN Lookup table 
Same VLANID can be mentioned in MAC Configuration Table and the VLANID also need to be configured in L2 Lookup table
 
These VLANID are used in L2 lookup table were for some MAC Address we utilized VLANID = 1 and for other MAC Addresses used VLANID = 2

in this configuration with respect to stream of VLANID = 1 is working fine able to Transmit and receive Message whatever the VLANID getting mentioned in Port 3 & Port 4 is configured that Configuration of Message is working fine 

Say suppose when i configure VLANID = 1 in Port 3 at the time the configuration with respect to that is working but the configuration with respect to VLANID = 2 is not working when i do vice versa its working fine 

The stream 2 is an UDP stream, which is coming around 30Mbps speed
what is the root cause of the issue ?

0 项奖励
回复
975 次查看
PavelL
NXP Employee
NXP Employee

Hello @Abrar_23 ,

UDP is fine for traffic testing. 30Mbps is also fine. Up to ~90% of max traffic load (in this case - egress queue) there should be no traffic drop.

I apologize for late responses, I have to prioritize my tasks.

Due to limited resources, customers which are using generic email accounts such as gmail.com or qq.com or similar have lower priorities. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly. Thank you for your understanding.

Best regards,

Pavel

0 项奖励
回复
971 次查看
Abrar_23
Contributor III

Hello @PavelL 
SWITCH - 1

Initially Created a Default VLANID 
VLANID = 0
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Disable all Ports
BC_DOMAIN = Disable all Ports
TAG_PORT = Disable all Ports
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 0

VLANID = 1
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4 -- ENABLE
BC_DOMAIN = Port 1,2,3,4 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 1

VLANID = 2
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4,5 -- ENABLE
BC_DOMAIN = Port 1,2,3,4,5 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 2

MAC Configuration Table 
Port 1 --> VLANPRIO = 7
VLANID = 1
Port 2 --> VLANPRIO = 7
VLANID = 2
Port 3 --> VLANPRIO = 7
VLANID = 3
Port 4 --> VLANPRIO = 7
VLANID = 4
Port 7 --> VLANPRIO = 3
VLANID = 2

SWITCH - 2
VLANID = 0
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Disable all Ports
BC_DOMAIN = Disable all Ports
TAG_PORT = Disable all Ports
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 0

VLANID = 1
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4 -- ENABLE
BC_DOMAIN = Port 1,2,3,4 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 1

VLANID = 2
VING_MIRR = Disable all Ports
VEGR_MIRR = Disable all Ports
VMEMB_PORT = Port 1,2,3,4,7 -- ENABLE
BC_DOMAIN = Port 1,2,3,4,7 -- ENABLE
TAG_PORT = Port 1,2
TYPE_ENTRY[1] = ENABLE
TYPE_ENTRY[0] = ENABLE
VLANID = 2

MAC Configuration Table 
Port 1 --> VLANPRIO = 7
VLANID = 1
Port 2 --> VLANPRIO = 7
VLANID = 2
Port 3 --> VLANPRIO = 7
VLANID = 3
Port 4 --> VLANPRIO = 7
VLANID = 4
Port 5 --> VLANPRIO = 3
VLANID = 2

I made the configuration changes above 
my CAN packets are getting Lost and CAMERA packets are getting streamed 
so what would be the root cause for packet loss even after configuring VLANID 
So what would be the ideal scenario to overcome the issue of Packet loss i understand CAMERA packets are flooding How to overcome this issue 
Regards
Abrar

 

标记 (1)
0 项奖励
回复
1,076 次查看
PavelL
NXP Employee
NXP Employee

Hello @Abrar_23 ,

I moved the post to the thread. I hope I will come with answer this week.

Thank you for your understanding.

Best regards,

Pavel

0 项奖励
回复