RW612 Matter Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RW612 Matter Controller

1,240 Views
Sanjiv
Contributor II

Hello. We are working with the VUI S2I platform and wish to integrate with MATTER devices. New to MATTER but have a room full of MATTER widgets working through HomePod (paired with QR codes). 

How does the RW612 integrate to the same platform to allow our RT106V board to control the assorted MATTER devices? Would you please share all documentation on this topic for our study?

From our understanding, the RW612 will need to act as the MATTER CONTROLLER? How is this controller informed of the surrounding matter devices we wish to control? For example, matter switch/bulb; matter dimmer; matter fan, etc.

Thanks.

Tags (2)
0 Kudos
Reply
2 Replies

1,216 Views
Sanjiv
Contributor II

Thank you. Will do. Just now, used the Google AI engine which offered an amazing summary on the whole process to do the same with the RW612. We will review for testing. 

0 Kudos
Reply

1,220 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. I would recommend checking our Matter | NXP Semiconductors web page.

For specific RW612, please refer to the official Matter examples, available on https://github.com/NXP/matter

Also, I would recommend checking this: RW612 Matter OTBR and Zigbee Bridge User Guide [UG10185].

 

Just extra information:

 

I would recommend checking all the news here: Smarter World Blog | NXP Semiconductors

 

Hope this helps.

 

Best Regards,

Ricardo

0 Kudos
Reply