RTC Interrupt Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC Interrupt Issue

1,410件の閲覧回数
yusupkhany
Contributor II

Hi All,

 

I am using PCF2127 RTC for my project and I am having issue with interrupt.

 

Enabling Minute interrupt using MI bit field in Control1 register. But MSF bit filed in Control2 register is always 0.

 

Interrupt signal is high in normal condition and the signal is going to low when interrupt generated.

But the MSF bit field is 0 and it’s not 1 when interrupt generated. 

 

I am facing same issue with seconds interrupt, alarm interrupt.

 

Looking forward for your prompt reply

 

Best Regards,

Yusup Khan

0 件の賞賛
返信
1 返信

1,347件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yusup,

I have never heard of such a problem and if the interrupt is generated the corresponding flag must be set.

pastedImage_1.png

Best regards,

Tomas

0 件の賞賛
返信