RTC Interrupt Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC Interrupt Issue

1,453 Views
yusupkhany
Contributor II

Hi All,

 

I am using PCF2127 RTC for my project and I am having issue with interrupt.

 

Enabling Minute interrupt using MI bit field in Control1 register. But MSF bit filed in Control2 register is always 0.

 

Interrupt signal is high in normal condition and the signal is going to low when interrupt generated.

But the MSF bit field is 0 and it’s not 1 when interrupt generated. 

 

I am facing same issue with seconds interrupt, alarm interrupt.

 

Looking forward for your prompt reply

 

Best Regards,

Yusup Khan

0 Kudos
Reply
1 Reply

1,390 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yusup,

I have never heard of such a problem and if the interrupt is generated the corresponding flag must be set.

pastedImage_1.png

Best regards,

Tomas

0 Kudos
Reply