RT600 sctimer capture function error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT600 sctimer capture function error

1,294件の閲覧回数
liwangzhao
Contributor I

I have been developing with the RT600 recently, using the SCTimer's capture function. An external pin triggers the SCTimer to capture a time into a register, which I then read in the interrupt. Most of the time, the moment I read from the interrupt is accurate, or at least the time is increasing incrementally. However, there is a small chance that the time in the CAP register for a certain frame is less than the time from the previous capture, but the next capture time returns to normal. Only this middle frame's time is incorrect. Does anyone know what might be causing this?

0 件の賞賛
返信
2 返答(返信)

1,213件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Unfortunately, there are no similar situations regarding this extrange issue.
Under what circumstances this happens? What is the state of OUTPUTDIRCTRL when this happens?

Best regards,
Omar

0 件の賞賛
返信

1,289件の閲覧回数
liwangzhao
Contributor I

there is no timer overflow happened,sure

0 件の賞賛
返信