RT600 sctimer capture function error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT600 sctimer capture function error

1,280 次查看
liwangzhao
Contributor I

I have been developing with the RT600 recently, using the SCTimer's capture function. An external pin triggers the SCTimer to capture a time into a register, which I then read in the interrupt. Most of the time, the moment I read from the interrupt is accurate, or at least the time is increasing incrementally. However, there is a small chance that the time in the CAP register for a certain frame is less than the time from the previous capture, but the next capture time returns to normal. Only this middle frame's time is incorrect. Does anyone know what might be causing this?

0 项奖励
回复
2 回复数

1,199 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Unfortunately, there are no similar situations regarding this extrange issue.
Under what circumstances this happens? What is the state of OUTPUTDIRCTRL when this happens?

Best regards,
Omar

0 项奖励
回复

1,275 次查看
liwangzhao
Contributor I

there is no timer overflow happened,sure

0 项奖励
回复