Hi,
We are using the RDDRONE-T1ADAPT media converter, but connection is continuously lost.
We are connecting to a Ethernet BroadR-Reach Phy Marvell 88Q2112, 1000Base-T1 and it seems not to support auto negotiation.
Is there a way to force RDDRONE-T1ADAPT into master mode? For instance by a special firmware?
Thanks
/Axel
Did you found the solution to get T1ADAPT always as a master?
Sorry, no. Not yet. We had very little time to look into a solution for that.
Are you also in need of being in a certain mode always?
Hi Axel,
I can see that RDDRONE-T1ADAPT should try slave mode first. If it fails, it starts trying master mode.
Regards,
Lukas
Hello @lukaszadrapa
Will the RDDRONE-T1ADAPT switch between master and slave perpetually? What is the frequency of that toggling between the two modes?
We're facing a condition where it sometimes takes several seconds to establish an Ethernet link with RDDRONE-T1ADAPT and I'm wondering if it could be due to this behavior.
Thanks!
Vic
Thanks for the info, @lukaszadrapa .
I think the problem is a bit more complex in our setup:
I think our client is closing down the connection and reopening it again, hence triggering an auto negotiate again on the RDDRONE-T1ADAPT.
I think our client is closing down, because it can't handle the auto negotiate.
Best would be to try a firmware version for RDDRONE-T1ADAPT, where it is always in MASTER mode.
Do you think this is possible?
Thanks,
/Axel
Hi Axel,
could you please create new case here?
https://support.nxp.com/s/?language=en_US
Write something like "for Lukas" to the description, it will be assigned to me.
Thanks,
Lukas