RDDRONE-T1ADAPT in master mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RDDRONE-T1ADAPT in master mode

1,333 Views
axjensen
Contributor I

Hi,

 

We are using  the RDDRONE-T1ADAPT media converter, but connection is continuously lost.

 

We are connecting to a Ethernet BroadR-Reach Phy Marvell 88Q2112, 1000Base-T1 and it seems not to support auto negotiation.

 

Is there a way to force RDDRONE-T1ADAPT into master mode? For instance by a special firmware?

 

 

Thanks

/Axel

0 Kudos
Reply
7 Replies

1,194 Views
kkonopczynski
Contributor I

Did you found the solution to get T1ADAPT always as a master?

0 Kudos
Reply

1,166 Views
axjensen
Contributor I

Sorry, no. Not yet. We had very little time to look into a solution for that. 

 

Are you also in need of being in a certain mode always?

 

 

 

0 Kudos
Reply

1,321 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Axel,

I can see that RDDRONE-T1ADAPT should try slave mode first. If it fails, it starts trying master mode.

Regards,

Lukas

777 Views
wlan
Contributor III

Hello @lukaszadrapa 

Will the RDDRONE-T1ADAPT switch between master and slave perpetually? What is the frequency of that toggling between the two modes?

We're facing a condition where it sometimes takes several seconds to establish an Ethernet link with RDDRONE-T1ADAPT and I'm wondering if it could be due to this behavior.

Thanks!

Vic

0 Kudos
Reply

1,317 Views
axjensen
Contributor I

Thanks for the info, @lukaszadrapa .

I think the problem is a bit more complex in our setup:

 

I think our client is closing down the connection and reopening it again, hence triggering an auto negotiate again on the RDDRONE-T1ADAPT.

 

I think our client is closing down, because it can't handle the auto negotiate.

Best would be to try a firmware version for RDDRONE-T1ADAPT, where it is always in MASTER mode.

 

Do you think this is possible?

 

Thanks,

/Axel

 

 

 

0 Kudos
Reply

1,312 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Axel,

could you please create new case here?

https://support.nxp.com/s/?language=en_US

Write something like "for Lukas" to the description, it will be assigned to me.

Thanks,

Lukas

0 Kudos
Reply

1,308 Views
axjensen
Contributor I

@lukaszadrapa:

 

Thanks.

Case Number : 00485140

0 Kudos
Reply