Questions abot MPC8313E-RDB card.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions abot MPC8313E-RDB card.

2,387件の閲覧回数
SMaybisher
Contributor I
Hi, I'm new in PowerPC. I'm looking for the MPC8313E-RDB card for beginning. My problem is that I don't have possibility for buying a debugger and then I want to load to RAM and run.
 
Is possible to do it?
If by mistake I'll erase the flash, is possible without debugger to burn it?
 
Thanks in advance.
 
S. Maybisher
0 件の賞賛
返信
2 返答(返信)

1,494件の閲覧回数
genuap
NXP Employee
NXP Employee
Nope - sorry. If you blow away the flash, you need a debugger to re-flash it.

It should ship with uboot in the flash - which should allow you to update uboot / Linux at least.


0 件の賞賛
返信

1,494件の閲覧回数
TedMarshall
Contributor II
Not quite true.  If you erase u-boot from the flash, you can boot from the I2C EEPROM which (at least on recent boards) contains an emergency flash load program.  This will allow you to use a terminal emulator with the kermit protocol to reburn u-boot.

See the Getting Started guide for more details.  In the rev. 1 document, it's section 3.2.
0 件の賞賛
返信