Question about NXP S32v234 plattform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about NXP S32v234 plattform

1,154件の閲覧回数
dortlearner
Contributor I

I'm using nxp s32v234 for multi-core parallel testing but have noticed a performance drop when running dual-core under the same cluster compared to single-core runs, and no drop when running with all cores. The test is each core running a separate application at the same time, The problem is that the performance degradation appears when running dual cores in the same cluster but disappears when running all cores. I'm assuming it could be an issue with the app itself used for testing or a component that plays a role in synchronising when running on multiple cores. Can anyone help me with this?

0 件の賞賛
返信
2 返答(返信)

1,136件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Correct! there are some issue in synchronization when changes from two cores but, avoid this by change between one core or four core. This correspond to errata ERR050767.

Regards

0 件の賞賛
返信

1,126件の閲覧回数
dortlearner
Contributor I

Thanks a lot for your reply. It really helps.

0 件の賞賛
返信