QSPI controller as SPI controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QSPI controller as SPI controller

1,262件の閲覧回数
Nareshvarikuntla
Contributor III

Dear NXP,

I need additional SPI controller for my board based on LS1046. So I would like use existing QSPI controller as SPI controller.

Is it possible to configure QSPI controller as SPI controller. If yes, Please share relevant information on it.

Regards,

Naresh V. 

タグ(2)
0 件の賞賛
返信
1 返信

1,251件の閲覧回数
ufedor
NXP Employee
NXP Employee

qSPI can work with non-flash device as long as it meets the timing spec. You can have up to 16 LUT sequences to deal with different slaves, which is not necessary flash devices.

qSPI does not support Mode 1 operation as it drives data on falling edge and samples data on rising edge.

qSPI does not support slave mode.

Refer to the QorIQ LS1046A Reference Manual, 27.6.3.5 Issuing SFM Commands and the following presentation:

https://www.nxp.com/webapp/Download?colCode=FTF-NET-F0008&location=null

 

0 件の賞賛
返信