QSPI controller as SPI controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI controller as SPI controller

1,298 Views
Nareshvarikuntla
Contributor III

Dear NXP,

I need additional SPI controller for my board based on LS1046. So I would like use existing QSPI controller as SPI controller.

Is it possible to configure QSPI controller as SPI controller. If yes, Please share relevant information on it.

Regards,

Naresh V. 

Tags (2)
0 Kudos
Reply
1 Reply

1,287 Views
ufedor
NXP Employee
NXP Employee

qSPI can work with non-flash device as long as it meets the timing spec. You can have up to 16 LUT sequences to deal with different slaves, which is not necessary flash devices.

qSPI does not support Mode 1 operation as it drives data on falling edge and samples data on rising edge.

qSPI does not support slave mode.

Refer to the QorIQ LS1046A Reference Manual, 27.6.3.5 Issuing SFM Commands and the following presentation:

https://www.nxp.com/webapp/Download?colCode=FTF-NET-F0008&location=null

 

0 Kudos
Reply