Programming the OTP options on AR6000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming the OTP options on AR6000

2,270件の閲覧回数
nick_norman
Contributor I

Although the datasheet shows what options can be OTP into an AR6000 alternator regulator, I can’t see where it says how this programming is actually done by the user. Is there another document that covers the OTP programming of AR6000?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,054件の閲覧回数
devonna_dorton
NXP Employee
NXP Employee

I am looking for the programming specifications for NXP AR6000 to provide to one of our device programming partners.

0 件の賞賛
返信

2,218件の閲覧回数
nxf54943
NXP Employee
NXP Employee

Hello Nick,
Sorry, but the information you are requesting is treated as confidential info at this time and requires a disclaimer between your company and NXP.
Naturally, we cannot discuss this with you in public, this requires to be handled as a support ticket. In the following link you'll be able to see the steps you need to follow in order to submit one: https://community.nxp.com/docs/DOC-329745 
We will stop following this thread and contact you by email to further communicate about the technical question.

Kind regards,
Andrea

-------------------------------------------------------------------------------
Note:
This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore
-------------------------------------------------------------------------------

0 件の賞賛
返信