Programming MMPF0200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming MMPF0200

2,666件の閲覧回数
max123
Contributor I

Hi,

we have trouble sourcing a preprogrammed Version of the MMPF0200 (F6 Variant). Therefore, I consider programming MMPF0200NP. I thought about using the following Hardware:

KITPF0100SKTEVBE (Adapter for QFN-56), KITPFPGMEVME (PMIC-Programmer).

The Kit claims to be for MMPF0100, but since the chips are very similar: Will this Kit and the software work for MMPF0200?

Can this be used to read the settings of an existing MMPF0200F6 chip and program it into a MMPF0200NP?

Thanks for any help in advance!

0 件の賞賛
返信
2 返答(返信)

2,623件の閲覧回数
max123
Contributor I

Thank you, that answers my question!

0 件の賞賛
返信

2,656件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Yes, KITPF0100SKTEVBE (Adapter for QFN-56), KITPFPGMEVME (PMIC-Programmer) are compatible and can be used to program the PF0200 PMIC

 

Yes, if you place a F6 PMIC on the socket board, you can read and export the current configuration, to save it using the PFGUI4.0. Then you place a NP unprogrammed version and load the F6 configuration to OTP program it. Check section 5.9 of the GUI User Guide: https://www.nxp.com/docs/en/user-guide/KTPFSWUG4.pdf

Regards,

Jose

0 件の賞賛
返信