Problem while running the QEMU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem while running the QEMU

5,120 Views
dibyarekha
Contributor IV

I am using LS1043A processor , I want to execute the emulator.

I am running the command ./qemu-system-aarch64 

it is giving an error showing 

aarch64-binfmt-P: Could not open '/lib/ld-linux-aarch64.so.1': No such file or directory

Please help me how can I use the qemu

0 Kudos
Reply
3 Replies

5,046 Views
June_Lu
NXP TechSupport
NXP TechSupport

I am sorry to say You that X86 is not supported on this helpdesk.
For X86 support. Please post this issue on vendor of X86 chip directly for support.

0 Kudos
Reply

5,084 Views
June_Lu
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

5,054 Views
dibyarekha
Contributor IV

Thanks for the response, Actually I don't have my target board. I want to use it in my system . Basically, I want QEMU in my host kernel system which is of x86-64 arch, but QEMU should work for aarch64. Is it possible?

 I am running the command in the following path

flexbuild_lsdk2108/build/rfs/rootfs_lsdk2108_ubuntu_main_arm64/usr/bin/

in this path I am getting the output as not a dynamic executable

The way you mentioned, if I am running the command in the same way, I am getting the following result

~$ ldd /usr/bin/qemu-system-aarch64
linux-vdso.so.1 (0x00007ffc645fb000)
libfdt.so.1 => /lib/x86_64-linux-gnu/libfdt.so.1 (0x00007fd636650000)
libz.so.1 => /lib/x86_64-linux-gnu/libz.so.1 (0x00007fd636634000)
libpixman-1.so.0 => /lib/x86_64-linux-gnu/libpixman-1.so.0 (0x00007fd635155000)
libpng16.so.16 => /lib/x86_64-linux-gnu/libpng16.so.16 (0x00007fd63511a000)
libjpeg.so.8 => /lib/x86_64-linux-gnu/libjpeg.so.8 (0x00007fd635099000)
libgnutls.so.30 => /lib/x86_64-linux-gnu/libgnutls.so.30 (0x00007fd634eae000)
libsasl2.so.2 => /lib/x86_64-linux-gnu/libsasl2.so.2 (0x00007fd636617000)
libpmem.so.1 => /lib/x86_64-linux-gnu/libpmem.so.1 (0x00007fd634e5a000)
libseccomp.so.2 => /lib/x86_64-linux-gnu/libseccomp.so.2 (0x00007fd634e3a000)
libnuma.so.1 => /lib/x86_64-linux-gnu/libnuma.so.1 (0x00007fd63660a000)
libgio-2.0.so.0 => /lib/x86_64-linux-gnu/libgio-2.0.so.0 (0x00007fd634c62000)
libgobject-2.0.so.0 => /lib/x86_64-linux-gnu/libgobject-2.0.so.0 (0x00007fd634c02000)
libglib-2.0.so.0 => /lib/x86_64-linux-gnu/libglib-2.0.so.0 (0x00007fd634ac8000)
librdmacm.so.1 => /lib/x86_64-linux-gnu/librdmacm.so.1 (0x00007fd634aa9000)
libibverbs.so.1 => /lib/x86_64-linux-gnu/libibverbs.so.1 (0x00007fd634a86000)
libzstd.so.1 => /lib/x86_64-linux-gnu/libzstd.so.1 (0x00007fd6349b7000)
libslirp.so.0 => /lib/x86_64-linux-gnu/libslirp.so.0 (0x00007fd634996000)
libudev.so.1 => /lib/x86_64-linux-gnu/libudev.so.1 (0x00007fd63496c000)
liburing.so.2 => /lib/x86_64-linux-gnu/liburing.so.2 (0x00007fd6365ff000)
libgmodule-2.0.so.0 => /lib/x86_64-linux-gnu/libgmodule-2.0.so.0 (0x00007fd634965000)
libnettle.so.8 => /lib/x86_64-linux-gnu/libnettle.so.8 (0x00007fd63491f000)
libfuse3.so.3 => /lib/x86_64-linux-gnu/libfuse3.so.3 (0x00007fd6348e0000)
libaio.so.1 => /lib/x86_64-linux-gnu/libaio.so.1 (0x00007fd6348db000)
libstdc++.so.6 => /lib/x86_64-linux-gnu/libstdc++.so.6 (0x00007fd634600000)
libm.so.6 => /lib/x86_64-linux-gnu/libm.so.6 (0x00007fd634519000)
libgcc_s.so.1 => /lib/x86_64-linux-gnu/libgcc_s.so.1 (0x00007fd6348bb000)
libc.so.6 => /lib/x86_64-linux-gnu/libc.so.6 (0x00007fd634200000)
/lib64/ld-linux-x86-64.so.2 (0x00007fd63666e000)
libp11-kit.so.0 => /lib/x86_64-linux-gnu/libp11-kit.so.0 (0x00007fd6340c5000)
libidn2.so.0 => /lib/x86_64-linux-gnu/libidn2.so.0 (0x00007fd63489a000)
libunistring.so.2 => /lib/x86_64-linux-gnu/libunistring.so.2 (0x00007fd633f1b000)
libtasn1.so.6 => /lib/x86_64-linux-gnu/libtasn1.so.6 (0x00007fd634880000)
libhogweed.so.6 => /lib/x86_64-linux-gnu/libhogweed.so.6 (0x00007fd634838000)
libgmp.so.10 => /lib/x86_64-linux-gnu/libgmp.so.10 (0x00007fd634497000)
libndctl.so.6 => /lib/x86_64-linux-gnu/libndctl.so.6 (0x00007fd634470000)
libdaxctl.so.1 => /lib/x86_64-linux-gnu/libdaxctl.so.1 (0x00007fd63482b000)
libmount.so.1 => /lib/x86_64-linux-gnu/libmount.so.1 (0x00007fd63442a000)
libselinux.so.1 => /lib/x86_64-linux-gnu/libselinux.so.1 (0x00007fd633eef000)
libffi.so.8 => /lib/x86_64-linux-gnu/libffi.so.8 (0x00007fd633ee2000)
libpcre.so.3 => /lib/x86_64-linux-gnu/libpcre.so.3 (0x00007fd633e6c000)
libnl-3.so.200 => /lib/x86_64-linux-gnu/libnl-3.so.200 (0x00007fd633e49000)
libnl-route-3.so.200 => /lib/x86_64-linux-gnu/libnl-route-3.so.200 (0x00007fd633dc6000)
libuuid.so.1 => /lib/x86_64-linux-gnu/libuuid.so.1 (0x00007fd633dbd000)
libkmod.so.2 => /lib/x86_64-linux-gnu/libkmod.so.2 (0x00007fd633da1000)
libblkid.so.1 => /lib/x86_64-linux-gnu/libblkid.so.1 (0x00007fd633d6a000)
libpcre2-8.so.0 => /lib/x86_64-linux-gnu/libpcre2-8.so.0 (0x00007fd633cd3000)
liblzma.so.5 => /lib/x86_64-linux-gnu/liblzma.so.5 (0x00007fd633ca8000)
libcrypto.so.3 => /lib/x86_64-linux-gnu/libcrypto.so.3 (0x00007fd633800000)

0 Kudos
Reply