Problem while loading code to flash(Failed to enter into background mode)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem while loading code to flash(Failed to enter into background mode)

1,750件の閲覧回数
mohammedshibin
Contributor I

Hai,

I am using PXS3020 for my project. I was testing the peripherals' functionality. I am using PE Micro multilink universal for debugging.

Everything was fine until today morning. Now I am not able to load the executable file into flash memory. I did not change anything in code from yesterday.  The screenshot of the error message is attached.

The peripheral that I enabled last is FlexPWM (Enabled Auxillary clock 0 - 16 MHz Internal RC Oscillator), and with PWM it was working until yesterday night.

Does auxiliary clock 0 create any problem? Kindly help me to solve the issue.

Thanks & Regards,

Mohammed Shibin

0 件の賞賛
返信
1 返信

1,646件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Just to close this thread - we were informed by customer that the problem was caused by FPGA which was holding the the reset pin low.

Lukas

0 件の賞賛
返信