Problem in generating IF(KHz) using SA612A mixer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in generating IF(KHz) using SA612A mixer

1,185 次查看
sanketpatel2020
Contributor I

Hi! Greetings!

I posted following query to NXP "Wireless Connectivity" discussion portal. I am not sure if it was appropriate place for my question. Hence posting it again here (in "other NXP solutions". Hopefully it covers RF too). Please go through it.

I have started working on SA612A mixer. Since many days, I have been struggling in generating IF (KHz) output.

NXP SA612A pin description (A quick reference so that you don't have to refer to the datasheet):

Pin1,2: differential RF input pins

Pin3: Ground

Pin4,5: differential IF output pins

Pin6,7: LO differential input

Pin8: +5V

My circuit configuration and problem detail:

  • 44.94MHz RF applied to pin1 through DC blocking capacitor. Pin2 is grounded via capacitor. RF signal level on pin1 is: <-15dBm (200mV peak to peak into 1.5kOhm input resistance of SA612) (<-15dBm ensures linear operating range considering IIP3) (at later stage I decreased the RF power further to 20mV rms, to make it operate in linear range)
  • 44.88MHz LO applied to pin 6, pin7 left open as suggested in datasheet/ application note:AN1993. LO level on pin6 is: 230mV peak to peak (as per datasheet, it has to be 200mV to 300mV peak to peak) (at later stage I also went for 224mV rms LO input)
  • Expecting to see 60Kz output (difference frequency) peak in the spectrum analyzer.

60KHz signal seems totally immersed in the noise, not a peak at all, what can be the reason? Tried with other frequencies as well.

Please share your views on this.

Regards,

Sanket

标签 (1)
  • RF

0 项奖励
回复
1 回复

1,011 次查看
andrei_skok
NXP Employee
NXP Employee

Please create a Service request.

How I could create a Service Request?

Please provide in Service request your schematics, Input and Output traces.

0 项奖励
回复