PowerPC performance questions.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PowerPC performance questions.

3,483 Views
Ze
Contributor I

I see a large number of PowerPC processors (i.e. 8240, 7410, 750, 970, etc.) mentioned in the literature from Freescale and others.  Is there any summary available of the relative performance of different processors?  I know actual clock speed, board design, software application, and multiple other variables all impact the final answer.  It still seems it should be possible to make some generalizations (e.g. processor X is typically 20% faster than processor Y).

Tags (1)
0 Kudos
Reply
1 Reply

1,339 Views
genuap
NXP Employee
NXP Employee

Attached is a presentation from the Freescale Technology Forum from 2005 that might help.

 ... Paul

 

e300_e500_e600_Comparison.pdf

Message Edited by t.dowe on 2009-10-20 01:07 PM
0 Kudos
Reply