PowerPC performance questions.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PowerPC performance questions.

3,494件の閲覧回数
Ze
Contributor I

I see a large number of PowerPC processors (i.e. 8240, 7410, 750, 970, etc.) mentioned in the literature from Freescale and others.  Is there any summary available of the relative performance of different processors?  I know actual clock speed, board design, software application, and multiple other variables all impact the final answer.  It still seems it should be possible to make some generalizations (e.g. processor X is typically 20% faster than processor Y).

タグ(1)
0 件の賞賛
返信
1 返信

1,350件の閲覧回数
genuap
NXP Employee
NXP Employee

Attached is a presentation from the Freescale Technology Forum from 2005 that might help.

 ... Paul

 

e300_e500_e600_Comparison.pdf

Message Edited by t.dowe on 2009-10-20 01:07 PM
0 件の賞賛
返信