Power level Control of MMZ09332BT1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Power level Control of MMZ09332BT1

1,296 次查看
antonjanovsky
Contributor I

Hi

I am planning to use your #MMZ09332BT1 RF AMP in a new design.

Would it be possible to change the bias voltage or any of the VCC's voltage to manipulate the gain but keep the amp out of any saturation points? (I basically want to make an ALC for different power levels , EG  low, medium and high power)

If so is there possibly some information regarding voltage to gain ration?

Regards

Anton

标签 (1)
  • RF

标记 (1)
0 项奖励
回复
1 回复

1,072 次查看
LPP
NXP Employee
NXP Employee

MMZ09332BT1 is not suitable for variable gain application.

Gate bias current value is set to provide best linearity of the amplifier. If you reduce gate bias current, small signal gain will go down but the large signal gain will not change.  So, the power gain versus output power will not be linear.

If you alter drain bias voltage, the amplifier would require different impedance matching network.

My suggestion is to use MMT20303H Digital Step Attenuator or BGA7204 variable gain amplifier to alter the gain.

https://www.nxp.com/products/rf/control-circuits/attenuators/50-4000-mhz-3-bit-1-db-lsb-digital-step...

https://www.nxp.com/products/rf/rf-amplifiers-low-medium-power/variable-gain-amplifiers:MC_50948


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复