Power Divider

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Divider

1,403 Views
nxf41527
NXP Employee
NXP Employee

I have a RF signal which i need to provide to 2 different inputs. Basically the same amplitude has to be provided from the same signal source , and they should be closely phase matched. I thought i could use a Power divider but that is not available as a board component. How else can I send the same signal to 2 different inputs with the same voltage ? The BW I am interested in is max of 3GHz .In simple words , I just need to copy my signals into both inputs without a considerable phase difference. 

0 Kudos
Reply
1 Reply