Power Divider

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Power Divider

1,405 次查看
nxf41527
NXP Employee
NXP Employee

I have a RF signal which i need to provide to 2 different inputs. Basically the same amplitude has to be provided from the same signal source , and they should be closely phase matched. I thought i could use a Power divider but that is not available as a board component. How else can I send the same signal to 2 different inputs with the same voltage ? The BW I am interested in is max of 3GHz .In simple words , I just need to copy my signals into both inputs without a considerable phase difference. 

0 项奖励
回复
1 回复