Portability of NXP thread for K32W

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Portability of NXP thread for K32W

710 次查看
sd05
Contributor III

Hello Community,

I had this doubt may be a stupid one but want to clear that if the NXP thread available with KW41Z SDK the lib

SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_br_cm0.a
SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_cm0.a
SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_ed_cm0.a

are platform specific?
As we have openthread which has a abstraction is it same with NXP thread?

Also where I can get NXP Thread stack source as what i can find are library?
Thanks!!

标记 (1)
0 项奖励
回复
1 回复

676 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. The files available for KW41Z are the ones you have in the SDK.

For K32W, you should use the OpenThread Stack available in the SDK and here: https://github.com/openthread/ot-nxp

 

Regards,

Ricardo

0 项奖励
回复