Portability of NXP thread for K32W

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Portability of NXP thread for K32W

710件の閲覧回数
sd05
Contributor III

Hello Community,

I had this doubt may be a stupid one but want to clear that if the NXP thread available with KW41Z SDK the lib

SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_br_cm0.a
SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_cm0.a
SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_ed_cm0.a

are platform specific?
As we have openthread which has a abstraction is it same with NXP thread?

Also where I can get NXP Thread stack source as what i can find are library?
Thanks!!

タグ(1)
0 件の賞賛
返信
1 返信

676件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. The files available for KW41Z are the ones you have in the SDK.

For K32W, you should use the OpenThread Stack available in the SDK and here: https://github.com/openthread/ot-nxp

 

Regards,

Ricardo

0 件の賞賛
返信