Pin connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin connection

3,496件の閲覧回数
Amiliy
Contributor I

Part:TDA8932BTW/N2,118 ,Is it normal that pins 1, 16, 17 and 32 are not connected by X-ray? Please help to give an explanation, thanks!TDA8932BTWN2,118.png

0 件の賞賛
返信
4 返答(返信)

3,445件の閲覧回数
Wilma
Contributor I

A pin joint is a connection between two objects that allows only relative rotation about a single axis. All translations as well as rotations about any other axis are prevented — the joint therefore has one degree of freedom (1-DOF).

rapidfs.com

0 件の賞賛
返信

3,450件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Are these 1, 16, 17 and 32pins  electric connected together when you test this part?

0 件の賞賛
返信

3,434件の閲覧回数
Amiliy
Contributor I

Only 1 pin is connected, 16,17,32 are not connected

0 件の賞賛
返信

3,422件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please see X-RAY picture attached.

0 件の賞賛
返信