Part Marking on PCA9506

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Part Marking on PCA9506

2,571件の閲覧回数
h_lorenz
Contributor I

Hi NXP-Team,

we are using the PCA9506 on a controller board in a application similar to automotive.

This control unit is in production for 2 years.

Now we have a problem with the I2C communication of some  units, we recently produced. 

The behaviour of PCA9506 with the part marking "CMZ110 02" is different to parts with the marking "CRR836 04".

See attached pictures.

I didn't found information respective to the meaning of these markings.

Can you give me some information to the meaning?

Are there changes in function between the 2 different parts?

Kind regards

Heiko Lorenz

タグ(2)
0 件の賞賛
返信
1 返信

2,503件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Heiko,

 

In order to assist with the requested information, please create a support ticket request.

 

Have a great day,

Paulina

0 件の賞賛
返信