PTN3356 reference design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3356 reference design

Jump to solution
1,844 Views
masahirokiniwa
Contributor IV

Hi,

I checked PTN3356 reference design in data sheet and application note(AN11590).

And I have two questions about their reference design as below.

1. In Fig4 of the data sheet, VDD_3V3 and GND are connected by FB. But they are not used in Fig5.

- Are they OPTION DESIGN as ESD protection and PI filter?

- Are they necessary only for DC to DC converter mode?  

pastedImage_1.pngpastedImage_2.png

2. In Fig4 and 5, VBUCK_1V5 is connected to GND by 4.7uF capacitor.

    I think that it is smoothing capacitor for SWOUT.

    Is it necessary for LDO mode? If it's necessary to both mode, could you tell me the purpose of it?

pastedImage_3.png

Best regards,

M.Kiniwa

1 Solution
1,729 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

For your question1:

The FB is optional for both modes.

For your question2:

4.7uF is the output capacitor which can stabilize the output voltage.

View solution in original post

1 Reply
1,730 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

For your question1:

The FB is optional for both modes.

For your question2:

4.7uF is the output capacitor which can stabilize the output voltage.