PN7150 Security level depending on Modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Security level depending on Modes

ソリューションへジャンプ
1,708件の閲覧回数
andy_kim
Contributor IV

Hello,

We are planning to apply PN7150 to our product.

A Security is important factor in our product.

I wonder if there is a different security level according to NFC communication Modes(Read/Write mode, Peer to Peer mode and Card Emulation mode).

Which mode do we can implement the most strong security level among them?

 

Best regards,

Andy

0 件の賞賛
返信
1 解決策
1,694件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @andy_kim ,

 

To add security features, you may use a SAM with PN7150, please kindly refer to https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-sam/mifare-sam-av3:MIFSAMAV3 for details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,695件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @andy_kim ,

 

To add security features, you may use a SAM with PN7150, please kindly refer to https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-sam/mifare-sam-av3:MIFSAMAV3 for details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信