PCF8563T register initialization value after a complete power-down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8563T register initialization value after a complete power-down

Jump to solution
1,368 Views
Louis1916
Contributor III

The customer tested that when the power supply VDD is powered off to 0.3V, the read time of the external device is 2080/9/0, is this consistent with the default initialization value of the design? Or is it dynamic random? Thank you!

0 Kudos
Reply
1 Solution
1,355 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个问题是不是我们在case里面讨论过了?还是客户又有新发现了目前?

View solution in original post

0 Kudos
Reply
1 Reply
1,356 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个问题是不是我们在case里面讨论过了?还是客户又有新发现了目前?

0 Kudos
Reply