PCF8563 pull-up resistors dimensioning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF8563 pull-up resistors dimensioning

1,957件の閲覧回数
cant
Contributor II

Hi all,

regarding the d.s. of the PCF8563, at pag. 29, tab. 29, are showed some minimum currents.

In order to dimension the pull-up resistors, it is not clear why are not showed the max values instead of the min ones, because it is open drain, so if the try to connect it directly to Vcc, isn't it in short circuit ?

Furthermore, in the UM10301 there are pull-up values, from whom you can deduct the currents values that are lower then in the tab 29.

Please can you clarify this aspect ?

Thanks a lot

0 件の賞賛
返信
2 返答(返信)

1,714件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Antonio,

In this case, the maximum current value for the IOL parameters would be maximum input current (Io) at any output mentioned on the Table28. Limiting values. You must place a pull-up resistor.

limiting_values.jpg

In order to dimension the pull-up resistors, I recommend that you go to Chapter 7.1 at the following document:

I2C-Bus specification and user manual​.

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信

1,363件の閲覧回数
HPFONE
Contributor I

Is there a recommended value range for the resistance of the pull-up resistor in PCF8563

0 件の賞賛
返信