PCF85263ATL/AX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF85263ATL/AX

1,329件の閲覧回数
ralexan
Contributor I

I am looking into using the PCF85263ATL/AX real time clock component.  During evaluation of the data sheet, I noticed that Pin-4(TS/CLK/INTB_n) is not connected if the input is not used; however, I cannot seem to find what to do with pin-9, INTA_n/CLK, and pin-8, CLK.  I don't just want to leave these unconnected so am looking for what is recommended for these pins if they are not being used.

0 件の賞賛
返信
1 返信

1,246件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

 

Hello Robert,

You can leave the Pin 9 INTA_n/CLK and Pin 8 CLC unconnected if they are not being used. You can also check the user manual UM10301 for NXP Real Time Clocks here (section 16). 

Have a great day,

Paulina

0 件の賞賛
返信