PCF8523, have source code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8523, have source code?

3,249 Views
jackylu
Contributor II

Hello,

PCF8523, have source code?

Please share,

Thanks.

0 Kudos
Reply
2 Replies

3,099 Views
ephraimschoenfe
Contributor II

Hi, 

There is, indeed no source code available  from NXP. The data sheet  is detailed enough to create a driver from scratch for the majority of the functionality. 

There are several source code repositories  that provide code for the PCF8523. 

Here below are some examples:

On Github:

The Arduino  library for PCF8523 is explained at 

All the examples above implement a subset of the functionality provided by the NXP chip PCF8523. 

We are searching for some examples of the use of the TIMER B and the INT2 line for a specific application. 

So far we have no success. 

This little note may help you to a starting point

0 Kudos
Reply

3,099 Views
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately we don't have source code but we have manual UM10301 for reference for hardware and software design.

0 Kudos
Reply