PCAL9722 100kOhm matching

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCAL9722 100kOhm matching

1,645件の閲覧回数
Fast
Contributor IV

Has anyone have an idea what the matching is for 100kOhm pull-up pull-down resistors?

First between pull-up and pull-down on same pin, and between pins?

If we knew what technology it is fabricated on, and size and type of element, we could hazard a guess? +/-10%?

0 件の賞賛
返信
4 返答(返信)

1,586件の閲覧回数
RafaR
NXP Employee
NXP Employee

Hello Fast

Well, I'm not sure I fully understand your questions. I'll respond to what I interpreted. Please let me know if you're referring to anything else in your questions.

 

All information related to the internal pull-ups of PCAL9722 is available under its datasheet:

RafaR_1-1749161516454.png

This internal pull-up/down are “weak”. If you are looking for tight tolerances, general recommendation is to use external “strong” pull-up/down.

 

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

0 件の賞賛
返信

1,566件の閲覧回数
Fast
Contributor IV

OK RafaR a fixed resistor is so cheap not worth worrying about matching.

0 件の賞賛
返信

1,547件の閲覧回数
Fast
Contributor IV

Actually I missed my point; quinary  base 5, is an option if pull resistance tolerable; 5 states, VDD, pull to VDD, float, pull to VSS, VSS. as you add ports the resolution increases much faster than trinary base 3. These potential DACs are good for comparator reference and hysteresis control.

0 件の賞賛
返信

1,629件の閲覧回数
RafaR
NXP Employee
NXP Employee

Hello Fast

I am starting to work on your case, I will contact you soon.

0 件の賞賛
返信