PCAL6416AHF misbehaves when machine starts.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCAL6416AHF misbehaves when machine starts.

1,628件の閲覧回数
Ashok_Sharma
Contributor II

Please find attached the video of misbehavior of I2C GPIO expander in field. It works fine when the machine is stopped!

The connections are as below:

gpio expandergpio expanderLEDsLEDs

The GPIO expander works fine when the machine starts,
The LEDs stop working!

The values of the control registers and data registers are printed on display for debug purpose, as seen in video top right and left corners.

(motor[17Hp] <- Supply -> SMPS -> Controller [buck converter] -> LCD module [buck converter])

タグ(3)
0 件の賞賛
返信
0 返答(返信)