PCAL6416AHF (HWQFN24 package thermal pad connection)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL6416AHF (HWQFN24 package thermal pad connection)

Jump to solution
950 Views
gwagner613
Contributor I

 

QFN24 package "exposed thermal pad" ... there is no information on whether this can / should / shouldn't be connected to GND.

I'm assuming it would be ok, but want to check.

Any issue with connecting the center pad to GND for PCAL6416AHF?

BR,

-- Glenn

0 Kudos
Reply
1 Solution
873 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Glenn,

The exposed pad underneath the PCAL6416AHF (HWQFN24) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

BRs, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
874 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Glenn,

The exposed pad underneath the PCAL6416AHF (HWQFN24) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

BRs, Tomas

0 Kudos
Reply