PCAL 6534 Power sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL 6534 Power sequence

1,173 Views
sohee
Contributor I

Is there any power that needs to be turn on first, VDD(P) or VDD(I2C_BUS)?

Does it need a power sequence for PCAL6534?

0 Kudos
Reply
3 Replies

1,157 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

VDD(P) should be powered first or at least not later than VDD(I2C_BUS). This ensures the internal circuits and registers are properly initialized before communication begins.

BRs, Tomas

0 Kudos
Reply

1,131 Views
sohee
Contributor I

Is there exact power sequence that contains timing?

Actually, VDD_I2C is powered first than VDD_P in design.

0 Kudos
Reply

1,121 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

There is no exact timing sequence specified. If VDD_I2C is powered first in your design, ensure that VDD_P ramps up promptly and reaches the POR threshold before any I²C communication is attempted. Note that the POR reset delay time is approximately 1 µs after VDD_P crosses the threshold. So to ensure reliable operation, allow a short delay (e.g. a few microseconds) after VDD_P is stable before initiating I²C transactions.

BRs, Tomas

0 Kudos
Reply