PCA9956B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,123件の閲覧回数
johnchen65
Contributor I

Hello

I'm looking for 7-segments driver.

I have some question regarding to current sinking in the datasheet page 41.

Is the parameter of Io(LEDn) meaning driving current out? or sinking current into the pin?

I didn't see any schematic for current output, the figure 20 is the current sinking.

Thanks,

John

0 件の賞賛
返信
1 解決策
2,020件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello John,

LED0 - LED23 are the LED current sink channels. These pins are connected to the LED cathodes.

Sink.JPG

Capture.JPG

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
2,021件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello John,

LED0 - LED23 are the LED current sink channels. These pins are connected to the LED cathodes.

Sink.JPG

Capture.JPG

Best regards,

Tomas