PCA9956B External Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9956B External Clock

1,922件の閲覧回数
davemarnatti
Contributor I

Greetings, I've used and external 4MHz clock to synchronize 4 pca9685 s, and would now like to do the same with the pca9956B.  The 9685 has an EXTCLK pin, a selection bit in MODE1, and even a prescaler to divide the clock down if desired.  I see a reference to external clocking in the 9956's datasheet (section 7.4), but no pin, control bit, or scaling capability.  Is what I want to do possible?  I need two of them to operate in lock step within a few nanoseconds, because I want to tie their per-channel outputs together in order to double the current.

0 件の賞賛
返信
2 返答(返信)

1,822件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello, Dave

 

The external clock mentioned in the datasheet, is referenced to the signal applied to the OE pin which can be used as a dimming or blinking control, setting LDRx = 01 will set fully ON the outputx, then you can blink/dim the outputx, applying a clock signal, since this pin can whether turn ON or OFF the device outputs.

 

Regards, Aldo

1,822件の閲覧回数
davemarnatti
Contributor I

Thanks for the clarification, Aldo,

Best regards,

Dave

0 件の賞賛
返信