PCA9701 and PCA9702

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,873件の閲覧回数
sasa_mesaric
Contributor I

Hi !

we are using PCA9701 and PCA9702.

Datasheet says :

Multiple PCA9701 or PCA9702 devices can be serially connected for monitoring a large number of switches by connecting the SDOUT of one device to the SDIN of the next device. SCLK and CS must be common among all devices and interrupt outputs may be tied together. No external logic is necessary because all the devices’ interrupt outputs are open-drain that function as ‘wired-AND’ and can simply be connected together to a single pull-up resistor.

Does this mean that we can connect  one PCA9701 and one PCA9702 together like described above or only PCA9701 can be connected together with another PCA9701 (same goes for PCA9702), so combination of PCA9701 and PCA9702 is not allowed?

Thank you !

Regards !

0 件の賞賛
返信
1 解決策
1,786件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This mean you can mixed connect PCA9701 and PCA9702 together.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,787件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This mean you can mixed connect PCA9701 and PCA9702 together.

0 件の賞賛
返信
1,786件の閲覧回数
sasa_mesaric
Contributor I

Thank you !

0 件の賞賛
返信