PCA9698BS Device Addressing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9698BS Device Addressing

Jump to solution
1,664 Views
ryan_smith
Contributor I

Hi,

I am utilizing the PCA9698BS I/O Expander in a design. For this part's device address I have the external strapping setup for address 0x20. But when I try to talk to address 0x20 over the I2C bus, I detect no I2C bus devices. But I actually detect the I/O Expander I2C bus on address 0x10. When I write commands to this address I am able to fully communicate with the PCA9698BS device. Why does the datasheet specify that the address is 0x20 (for the external strapping that I'm using), when address 0x10 works instead?? The device address 0x10 isn't even an option within the PCA9698BS datasheet.

Thanks,

Ryan

0 Kudos
Reply
1 Solution
1,646 Views
ErikaC
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
1,622 Views
ryan_smith
Contributor I

Hi Erika,

Thanks for sharing this post. It was my assumption that something such as bit shifting was happening. Thanks for confirming.

-Ryan

0 Kudos
Reply
1,647 Views
ErikaC
NXP TechSupport
NXP TechSupport
0 Kudos
Reply