PCA9617A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9617A

1,267 Views
n-ogawa
Contributor I
In the PCA9617A data sheet, is it necessary to have a high pulse after ACK on SDA in Figure 8.
When level conversion of data (part of slave register address) from SDAA to SDAB of PCA 9617A, the data may change  probably because there is not the high pulse.
0 Kudos
Reply
1 Reply

1,208 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Naoyuki,

It is common to have such a high pulse after the ACK and before the next data byte because the SDA line is no longer pulled low by the slave. During that time it is pulled high through a pull-up resistor. 

pastedImage_1.png

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos
Reply