PCA9614

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,722件の閲覧回数
sd23
Contributor I

How do we determine termination resistor values for PCA9614?

0 件の賞賛
返信
1 解決策
3,684件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sedef,

I would recommend you to take a look at the AN847 which includes the calculations of proper bus termination resistors.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,685件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sedef,

I would recommend you to take a look at the AN847 which includes the calculations of proper bus termination resistors.

Best regards,

Tomas

0 件の賞賛
返信
1,725件の閲覧回数
Mietto2
Contributor I

Hi,

I have a similar application with Vdd=3.3V on both sides, and Z0=100R.

Going through the app note, two questions arised:

1) The app note mentions the FAILSAFE bias = 200mV. What is that value with the PCA9614?

2) The app note do not consider 3 resistors on both sides of the cable, while the PCA9614 asks for that. What is the impact?

Best regards.

0 件の賞賛
返信
3,673件の閲覧回数
sd23
Contributor I

Thank you Thomas.

0 件の賞賛
返信
3,719件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

The termination resistor determined by the VCCA/VCCB setting,what're value of them in your side?

0 件の賞賛
返信
3,705件の閲覧回数
sd23
Contributor I

Both are 3.3V.

0 件の賞賛
返信