PCA85133 - LCD Driver -- Power up Issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA85133 - LCD Driver -- Power up Issue.

Jump to solution
2,353 Views
karuna_pcs
Contributor I

Hi All,

    We are facing problem with PCA85133 + LCD. Slave  does not acknowledged

Fclk - 2.5KHz

If i try to write the slave address 0x70, it is not ack....Please any one help us. 

0 Kudos
Reply
1 Solution
2,261 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karunakaran,

If you have a logic analyzer or an oscilloscope, could you please post here the picture illustrating the I2C traffic?

Also make sure you are using the correct I2C address depending on the voltage on the SA0 input.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
2 Replies
2,261 Views
karuna_pcs
Contributor I

Problem resolved.

0 Kudos
Reply
2,262 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karunakaran,

If you have a logic analyzer or an oscilloscope, could you please post here the picture illustrating the I2C traffic?

Also make sure you are using the correct I2C address depending on the voltage on the SA0 input.

Best regards,

Tomas

0 Kudos
Reply