PCA85133 - LCD Driver -- Power up Issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA85133 - LCD Driver -- Power up Issue.

ソリューションへジャンプ
2,360件の閲覧回数
karuna_pcs
Contributor I

Hi All,

    We are facing problem with PCA85133 + LCD. Slave  does not acknowledged

Fclk - 2.5KHz

If i try to write the slave address 0x70, it is not ack....Please any one help us. 

0 件の賞賛
返信
1 解決策
2,268件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karunakaran,

If you have a logic analyzer or an oscilloscope, could you please post here the picture illustrating the I2C traffic?

Also make sure you are using the correct I2C address depending on the voltage on the SA0 input.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,268件の閲覧回数
karuna_pcs
Contributor I

Problem resolved.

0 件の賞賛
返信
2,269件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karunakaran,

If you have a logic analyzer or an oscilloscope, could you please post here the picture illustrating the I2C traffic?

Also make sure you are using the correct I2C address depending on the voltage on the SA0 input.

Best regards,

Tomas

0 件の賞賛
返信