PCA85133 - LCD Driver -- Power up Issue.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCA85133 - LCD Driver -- Power up Issue.

跳至解决方案
2,366 次查看
karuna_pcs
Contributor I

Hi All,

    We are facing problem with PCA85133 + LCD. Slave  does not acknowledged

Fclk - 2.5KHz

If i try to write the slave address 0x70, it is not ack....Please any one help us. 

0 项奖励
回复
1 解答
2,274 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karunakaran,

If you have a logic analyzer or an oscilloscope, could you please post here the picture illustrating the I2C traffic?

Also make sure you are using the correct I2C address depending on the voltage on the SA0 input.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,274 次查看
karuna_pcs
Contributor I

Problem resolved.

0 项奖励
回复
2,275 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karunakaran,

If you have a logic analyzer or an oscilloscope, could you please post here the picture illustrating the I2C traffic?

Also make sure you are using the correct I2C address depending on the voltage on the SA0 input.

Best regards,

Tomas

0 项奖励
回复