PCA85063A second, minute alarms are not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA85063A second, minute alarms are not working

811件の閲覧回数
riteshpatel
Contributor II

Hi,

We are interfacing the NXP RTC PCA85063A chipset with the modified micro-controller. We would like to generate interrupt on INTB pin after 1 second of time.

For that, we are configuring the register with below values.

control_status_reg2 ( 0x01) = 0x80; /* 

reg_second_alarm (0x0B)  = 0x01; /* Enabled second alarm, alarm for 1 seconds, other register default values are disabled by default */

This should generate the alarm and generate an interrupt after 1 second. 

1) Please note that RTC time is proper and we are getting proper RTC data in this so it should generate the alarm signal. 

2) We have also verified by polling the control_reg_2 register that the value of AF is not set to 1. So, it means there is some issue with the configurations.

Please mention if we are missing any register configuration here.

Regards.

タグ(1)
0 件の賞賛
返信
1 返信

692件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Ritesh, 

First please accept our apologize for the delayed response. 

Are you still experiencing this issue?

Have a great day, 

Paulina

0 件の賞賛
返信