[P4080] : Error Unable to load RCW file - MPIC_reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[P4080] : Error Unable to load RCW file - MPIC_reset

1,540 次查看
Arathi
Contributor II

Hi NXP Support Team ,

We have a custom board with P4080 processor.
We are using trace32 application to load files.
While trying to load RCW file with T32 we are getting Running(MPIC_Reset) error message in status tab.

Attaching the error snapshot for your reference.

Can you please help me resolve this issue.

Regards,
Arathi

0 项奖励
回复
3 回复数

1,514 次查看
rweiss
Contributor V

I assume you were using the RCW override script from the demo folder. The override script contains an RCW that is suitable for the P4080 evaluation board. It may be necessary to change the RCW in the script so that it matches your hardware. Alternatively you could change the bootstrap configuration so that the processor is using a default configuration instead of reading the RCW from FLASH. In this default configuration, you should be able to connect (SYStem.Up) without RCW override script.

Best regards,
Reinhard

 

0 项奖励
回复

1,518 次查看
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

Sorry, we don't support Trace32, but you can upload a new RCW using only U-boot.
You can consult the steps to update the RCW following the link:

Programming a New U-boot, RCW, FMan Microcode | QorIQ SDK v2.0-1703 Documentation | NXP Semiconducto...

0 项奖励
回复

1,484 次查看
Arathi
Contributor II

Hi Team,

Thanks for your support.

On Debugging it is found that there was an inconsistency in one of the voltage supply to the processor.
Replacing the voltage regulator made us resolve this issue.

Thanks and regards,
Arathi

0 项奖励
回复