Optimizing Embedded Systems for Edge Computing with Rack Servers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Optimizing Embedded Systems for Edge Computing with Rack Servers

949 次查看
luciaonmatteo
Contributor III

Hello everyone,

I'm currently exploring options for optimizing embedded systems in edge computing environments and I wanted to reach out to this community for insights. Specifically, I'm looking at how to integrate powerful rack servers into systems that require real-time data processing at the edge.

I've been working on a project where we need to handle large volumes of data coming from IoT devices deployed in remote areas. Our goal is to minimize latency by processing data locally rather than sending it to a centralized data center. This is where rack servers come into play. Given their ability to support high-density hardware in a compact space, rack servers seem to be a great fit for edge computing applications.

However, the integration process hasn't been without challenges. One of the primary issues I've encountered is managing the power consumption and thermal dissipation of these servers when running high-performance tasks in an environment with limited cooling. Has anyone here had experience with configuring rack servers for edge computing?

I'd be especially interested to hear from those who have successfully used embedded systems alongside traditional server racks. Are there any best practices for balancing system reliability and performance? Also, if anyone has recommendations for specific models or configurations that are known for handling heavy edge computing tasks, I would greatly appreciate the input.

Looking forward to hearing your thoughts and experiences!

 

标签 (2)
0 项奖励
回复
1 回复

915 次查看
June_Lu
NXP TechSupport
NXP TechSupport

LX2160A Reference Design Board, see www.nxp.com/lx2160a-rdb

The LX2160A RDB (Reference Design Board) is a 1U rack-mount chassis form factor with a 2.2GHz LX2160A Rev 2.0 device.

  • Memory: two 288-pin DIMM slots, each populated with a 16GB 3200MT/s DDR4 UDIMM (for a total of 32GB).
  • Flash: 128MB NOR flash, 128GB eMMC, and an SD Slot populated with a 32GB SD card. For reliable operation of the RDB, the SD slot should always have a SD card in it, even if not used. This is related to the defeaturing of the 3.3V EVDD as noted above. The board can face long-term reliability problems if the SD slot is not populated.
  • SerDes1 (config 19): QSFP+ (40GE), two SFP+ (25GE), and two RJ45 USXGMII (10GE)
  • SerDes2 (config 5): x4 PCIe Gen3 slot and four SATA3.0
  • SerDes3 (config 2): x8 PCIe Gen3 slot
  • One USB Host Type A, one USB3.0 Type AB, two RS232, JTAG, two RGMII

 

Lx2160A's high performance and the thermal solution of the LX2160ARDB would be a good reference for you.

We provide thermal simulation models to customer to simulate the thermal solution under NDA.

Any point of particular interest to you please let me know.

Thanks

0 项奖励
回复