Optimising PCF8523T in Direct Switching Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Optimising PCF8523T in Direct Switching Mode

1,716件の閲覧回数
philsolomon
Contributor I

I am powering the VDD for the PCF8523 at 5Vdc and VBAT at 4.6Vdc. I am looking to use the "direct switching mode" to transition to VBAT when VDD is lost. The datasheet for the PCF8523 quotes:

* IDD = 150nA (typ) and 500nA (max) when configured as PM[2:0] = 111 and clock output disabled.

* IDD = 1200nA (typ) and 3600nA (max) when configured as PM[2:0] = 0000 and clock output enabled.

My application requires IDD = 500nA (max) but neither of the configurations above match my requirements which are "direct switching mode" enabled and "clock output disabled".

Can NXP please provide the equivalent data for the most efficient mode (in terms of maximum IDD) for the options for "direct switching mode" enabled and "clock output disabled".

Thank you,

Phil.

#PCF8523T

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,539件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Phil,

Thank you for your interest in the PCF8523T.

 

I am afraid we do not have the data specifically for the PCF8523T.

 

The current consumption will drop if CLKOUT is disabled. Also, the current consumption reduces with lower supply voltage.

 

With regards to the power management setting, the highest current consumption will be when PM[2:0]=000 and the lowest current consumption will be when PM[2:0]=111. The other PM settings will yield to lower current consumption than the PM[2:0]=000 setting, but not lower than the PM[2:0]=111 setting.

 

I hope it helps.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

1,539件の閲覧回数
philsolomon
Contributor I

Thank you for the feedback Tomas. It has provided me with which direction to head now.

0 件の賞賛
返信